This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any register in DM8167 which can be used to differ from DM8168?

Is there any register in DM8167 which can be used to differ from DM8168?

  • Hello,

    I do not think there is such a register, to check whether you are using DM8167 or DM8168 device. You can check the Part# (in example TMS320DM8167BCYG2, TMS320DM8167SCYG, TMS320DM8167SCYG2, TMS320DM8167SCYG4) to define if you are using DM8167 device.

    The only difference between DM8168 and DM8167 is that DM8167 does not have SGX graphics accelerator, so the SGX registers (see table 1-48 from the DM816x TRM) should not exist, thus not software accessible/configurable, for DM8167 device.

    Regards,

    Pavel