This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3 EVM: USB Device functionality in Full Speed mode



Hello all,

I am working with the OMAP3 EVM running Linux kernel 2.6.37 from PSP 04.02.00.07.  

My requirement is to have the USB OTG port configured as a device for CDC Ethernet support in Full Speed mode

To start with, I use the default kernel sources and the configuration (omap3_evm_defconfig) and am able to get CDC Ethernet working in High speed mode between the OMAP3 EVM and a host PC running Ubuntu 11.04.

I am able to ping between the EVM and the Linux PC, both ways. 

In order to configure the USB OTG controller in Full speed mode, I have made the following change in function musb_start of drivers/usb/musb/musb_core.c 

   /* put into basic highspeed mode and start session */
   musb_writeb(regs, MUSB_POWER, MUSB_POWER_ISOUPDATE
   | MUSB_POWER_SOFTCONN
   - | MUSB_POWER_HSENAB
   + /* | MUSB_POWER_HSENAB */
   /* ENSUSPEND wedges tusb */
   /* | MUSB_POWER_ENSUSPEND */
   );

With these changes, when I connect the OMAP3 EVM to the Host PC:

  • The PC detects the OMAP3 EVM as a full speed USB device
  • I am able to assign IP addresses to the usb0 interface on both the PC and the OMAP3 EVM

dmesg on the Host PC confirms this:

usb 2-1.2: new full speed USB device using ehci_hcd and address 37
usb 2-1.2: not running at top speed; connect to a high speed hub
cdc_ether 2-1.2:1.0: usb0: register 'cdc_ether' at usb-0000:00:1d.0-1.2, CDC Ethernet Device, da:cc:d1:cd:87:75

However, attempts to ping the Linux PC from the OMAP3 EVM results in failure.

dmesg on the Host PC shows the following logs:

usb0: no IPv6 routers present
hub 2-1:1.0: port 2 disabled by hub (EMI?), re-enabling...
usb 2-1.2: USB disconnect, address 37
cdc_ether 2-1.2:1.0: usb0: unregister 'cdc_ether' usb-0000:00:1d.0-1.2, CDC Ethernet Device
cdc_ether 2-1.2:1.0: usb0: can't clear rx halt, status -11
usb 2-1.2: new full speed USB device using ehci_hcd and address 38
usb 2-1.2: not running at top speed; connect to a high speed hub
cdc_ether 2-1.2:1.0: usb0: register 'cdc_ether' at usb-0000:00:1d.0-1.2, CDC Ethernet Device, da:cc:d1:cd:87:75
hub 2-1:1.0: port 2 disabled by hub (EMI?), re-enabling...
usb 2-1.2: USB disconnect, address 38
cdc_ether 2-1.2:1.0: usb0: unregister 'cdc_ether' usb-0000:00:1d.0-1.2, CDC Ethernet Device
usb 2-1.2: new full speed USB device using ehci_hcd and address 39
usb 2-1.2: not running at top speed; connect to a high speed hub
cdc_ether 2-1.2:1.0: usb0: register 'cdc_ether' at usb-0000:00:1d.0-1.2, CDC Ethernet Device, da:cc:d1:cd:87:75
cdc_ether 2-1.2:1.0: usb0: kevent 1 may have been dropped
cdc_ether 2-1.2:1.0: usb0: kevent 1 may have been dropped
hub 2-1:1.0: port 2 disabled by hub (EMI?), re-enabling...
usb 2-1.2: USB disconnect, address 39
cdc_ether 2-1.2:1.0: usb0: unregister 'cdc_ether' usb-0000:00:1d.0-1.2, CDC Ethernet Device
cdc_ether 2-1.2:1.0: usb0: can't clear rx halt, status -11
usb 2-1.2: new full speed USB device using ehci_hcd and address 40
usb 2-1.2: not running at top speed; connect to a high speed hub
cdc_ether 2-1.2:1.0: usb0: register 'cdc_ether' at usb-0000:00:1d.0-1.2, CDC Ethernet Device, da:cc:d1:cd:87:75
cdc_ether 2-1.2:1.0: usb0: kevent 1 may have been dropped
cdc_ether 2-1.2:1.0: usb0: kevent 1 may have been dropped
cdc_ether 2-1.2:1.0: usb0: kevent 1 may have been dropped
hub 2-1:1.0: port 2 disabled by hub (EMI?), re-enabling...
usb 2-1.2: USB disconnect, address 40
cdc_ether 2-1.2:1.0: usb0: unregister 'cdc_ether' usb-0000:00:1d.0-1.2, CDC Ethernet Device
cdc_ether 2-1.2:1.0: usb0: can't clear rx halt, status -11
usb 2-1.2: new full speed USB device using ehci_hcd and address 41
usb 2-1.2: not running at top speed; connect to a high speed hub
cdc_ether 2-1.2:1.0: usb0: register 'cdc_ether' at usb-0000:00:1d.0-1.2, CDC Ethernet Device, da:cc:d1:cd:87:75
usb0: no IPv6 routers present

Any pointers or guidance on what is wrong would be extremely helpful.

Thank you for your time

Warm regards,

Kanagesh