Hi,
From the OMAPL138 McBSP documentation, it states the following:
1.1 Purpose of the Peripheral
The primary use for the multichannel buffered serial port (McBSP) is for audio interface purposes. The McBSP is a specialized version of the McBSP peripheral used on other TI DSPs. The primary audio modes that are supported are the AC97 and IIS modes. In addition to the primary audio modes, the McBSP can be programmed to support other serial formats but is not intended to be used as a high-speed interface.
So can someone tell me what is special about the McBSP on the OMAP? Also, if I try to use it as a high-speed interface even though it says that it is not intended to be used that way, what limitations or issues will I run into?
Thanks,
Charles