Other Parts Discussed in Thread: AM3352, SYSBIOS
On the AM3352, is there any way to monitor the 2 Ethernet Port statistics separately and simultaneously? It appears that only the combined sum can be monitored.
Also
I am trying to find the best PMIC, comparing the TPS65910A1 and TPS65217C. The TPS65217C is fully characterized from -40C to 105C, great for Industrial comms. However, I cannot determine from the TPS65217C documentation if the device can be configured for an always-on application. In other words, our product will always be running full speed when 24V power is present, no sleep or low-power modes will be used.