Hello,
I am trying to discover the switch in my network. I am on a C6678 EVM.
I receive a port OK. So I am confident in the SERDES settings. I have pre-tested ackId alignment, maintanence write and maintence read routines. These can be found in my other posts. They work with a static configuration. So with them I change the destination id to 0xFF.
I can send a promiscuious maintanence read packet - out of power up - and receive a response from the switch.
However, I cannot align the ackids in order to do anything without a power cycle. Any promiscuisous write attempts return a time out error code. (in other words whether I just powered on or reloaded the emulator, I cannot get a promiscuisous write attempt to work.)
Do you think this is a problem with the settings in my switch or the settings on the DSP? Do I need to set a bit on the DSP to accept a promiscuious write response?
Is there a discovery algorithm available to reference?
thanks,
Brandy