This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDHC Compatible problem on DM3730 with Wince6.0

Hi,

     I am now in use of EVM2 with WinCE6.0. when I inserted a Kinston SD Card(SDHC class4 8G ) ,the system recognised it correct, but when i inserted a SanDisk SD card(SDHC class4 8G ), some of the SD card can't recognised, and the detail problems as follows:

1. when the kinston SD card formated with FAT32 on PC , and inserted into the Board, it can be recognised.

2. when some files copied into the SD card ,and inserted to the board again ,the SD card can't be recognised .

 

What's the problem with this?

Hope for your reply

Best regards

Liuyan from NovaStar