This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ruby on rails meet lighttpd on arago linux ...is it possible?!



Hi all,

basically , the features provided with the installation of the ti-sdk-am335x-evm-05.04.01.00 with the beagle bone board (booting with  NFS and tftp) include the possibility to manage and "customize" the lighttpd web server. Change the lighttpd.conf file inside /etc and so on.

Now , to improve the performance of the system  , I'd like to use ruby on rails and mySQL.

So, what is the best way to install those two tools in the system?!  any tips about this question are highly welcome :)

Thanks in advance

Marco