Other Parts Discussed in Thread: OMAP3530
Hi,
Omap3530Evm(Beagle Board): I want to add AACHEENC codec to codecserver and have a AAC-HEv2 encoding on device. So i download the AAC-HEv2 codec from ti website, add it to codec server and build it. The process of making codec server, get me a new cs.X64P file.
Then I "make" and "make install" entire dvsdk, dvsdk-demos and codecs. Hence, I have some new files in "targetfs" folder including cmem driver, dvsdk demos, codec server files and others.
Now, there are following problems:
1. When I copied the new made dvsdk-demo files to file system, and run loadmodules.sh it give this errors back to me:
Error Details.
# ./loadmodules.sh
CMEMK module: built on Jul 13 2010 at 09:03:04
Reference Linux version 2.6.32
.
.
dsplinkk: disagrees about version of symbol module_layout
insmod: error inserting 'dsplinkk.ko': -1 Invalid module format
BusyBox v1.16.1 (2010-07-12 18:43:40 JST) multi-call binary.
Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR
Create a special file (block, character, or pipe)
Options:
-m Create the special file using the specified mode (default a=rw)
TYPEs include:
b: Make a block device
c lpm_omap3530: Unknown symbol IPS_notify
or u: Make a character device
lpm_omap3530: Unknown symbol IPS_register
p: Make a named pipe (MAJOR and lpm_omap3530: Unknown symbol IPS_unregister
MINOR are ignored)
lpm_omap3530: Unknown symbol LDRV_PROC_setState
lpm_omap3530: Unknown symbol LDRV_PROC_getState
lpm_omap3530: Unknown symbol PMGR_PROC_getSymbolAddress
insmod: error inserting 'lpm_omap3530.ko': -1 Unknown symbol in module
2.I tried to copy a new complete rootfs and boot using mksdboot.sh file and it successfully completed. But boot-loader hangs:
Texas Instruments X-Loader 1.46 (Aug 16 2010 - 16:16:57)
Starting OS Bootloader...
3. I repeat this steps with dvsdk_4_00_02 and 4_03 but it never boots succesfully. When I use old boot files(u-boot,MLO and uImage) with recently made rootfs, following errors is generated and boot process no longer proceeded :
FATAL: Module omaplfb not found.
FATAL: Module bufferclass_ti not found.
BusyBox v1.13.2 (2011-12-23 00:31:29 IST) multi-call binary
Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR
Create a special file (block, character, or pipe)
Options:
-m Create the special file using the specified mode (default a=rw)
TYPEs include:
b: Make a block device
c or u: Make a character device
p: Make a named pipe (MAJOR and MINOR are ignored)
chmod: /dev/pvrsrvkm: No such file or directory
Starting SGX fixup for ES5.x
FATAL: Module cmemk not found.
FATAL: Module dsplinkk not found.
FATAL: Module lpm_omap3530 not found.
FATAL: Module sdmak not found.
numid=48,iface=MIXER,name='HeadsetL Mixer AudioL1'
; type=BOOLEAN,access=rw------,values=1
: values=on
numid=45,iface=MIXER,name='HeadsetR Mixer AudioR1'
; type=BOOLEAN,access=rw------,values=1
: values=on
Simple mixer control 'Headset',0
Capabilities: pvolume penum
Playback channels: Front Left - Front Right
Limits: Playback 0 - 3
Mono:
Front Left: Playback 3 [100%] [6.00dB]
Front Right: Playback 3 [100%] [6.00dB]
INIT: Id "S" respawning too fast: disabled for 5 minutes
NOW, Please say me, where I made mistakes and what I must do to?
How to install the kernel on dvsdk_4_03 psp package on device with appropriate boot files?
And should I updare boot partition of SD card for installing new filesystem files?
Thanks