Hi,
I am using WinCE7 BSP for OMAP4 family.
can we discuss any of the issues related to OMAP4 BSP here?
Regards,
GSR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Prashant Agarwal,
I haven't modified the either of them. Instead I choose two options
Hi GSR,
I have included these module only so can you share that NK.BIN you are getting is of which size because my config.bib NK size is specified as 72MB.
So in release build I am getting NK binary as 50 MB so it can accomodate within 72MB.
But in case of Debug Build I am getting 110MB NK image .
Or can you share the config.bib details what you are using for debug build.
Any help is appreciated.
Hi Prashant,
I didn't understood completely.
In my previous post I clearly said I haven't modified config.bib so even if I share config.bib it will contain default values only.
Try to remove unwanted SYSGEN components, so that you can have debug image within the range of 72MB.
Regards,
GSR
Hi GSR ,
I thought you are also getting the image size of about 110MB instead of less than 72MB thats why I asked you to share your config file.
But the problem is by removing some of the sysgen variable also the size is getting decreased by about 10-15 MB which is still more than 72MB so what else I should try to remove these problems.
Any help is appreciated.
Hi GSR,
One more doubt if you can help is,
While implementing KITL we are implementing through USB RNDIS.
So when I am connecting the USB cable from Board(Development) to Host(Desktop) then it is showing the device details and all but when we are checking it into device manager its showing that driver is not installed for that.
So whether do we need any host side driver for that if yes so from where we can get it.
Hi GSR ,
I tried to remove the sysgen component then performed the build release as well as debug.
So in that case release build is working fine but in debig build I am getting log as mentioned below and then its not booting up completely.
Windows CE SD X-Loader for OMAP4430
Built Jan 4 2013 at 10:36:22
Version 6.13.00
open ebootsd.nb0 file
jumping to ebootsd image
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Jan 4 2013 11:31:49
Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Jan 4 2013 at 11:36:56
EBOOT Version 1.5, BSP 6.13.00
BEFORE RETURN System ready!
Preparing for download...
INFO: Predownload....
WARN: Boot config wasn't found, using defaults
INFO: SW4 boot setting: 0x05
After default boot configuration
>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...
--------------------------------------------------------------------------------
Main Menu
--------------------------------------------------------------------------------
[1] Show Current Settings
[2] Select Boot Device
[3] Select KITL (Debug) Device
[4] Network Settings
[5] SDCard Settings
[6] Set Device ID
[7] Save Settings
[8] Flash Management
[0] Exit and Continue
Selection: 2
--------------------------------------------------------------------------------
Select Boot Device
--------------------------------------------------------------------------------
[1] LAN9115 MAC
[2] USBFn RNDIS
[3] NK from SDCard FILE
[0] Exit and Continue
Selection (actual LAN9115 MAC): 3
Boot device set to NK from SDCard FILE
--------------------------------------------------------------------------------
Main Menu
--------------------------------------------------------------------------------
[1] Show Current Settings
[2] Select Boot Device
[3] Select KITL (Debug) Device
[4] Network Settings
[5] SDCard Settings
[6] Set Device ID
[7] Save Settings
[8] Flash Management
[0] Exit and Continue
Selection: 0
BL_IMAGE_TYPE_BIN
Download file information:
-----------------------------------------------------------
[0]: Address=0x8c000000 Length=0x03462a18 Save=0x80000000
-----------------------------------------------------------
Download file type: 1
<> Record [ 0 ] dwRecAddr = 0x8c000000, dwRecLen = 0x4
<> Record [ 1 ] dwRecAddr = 0x8c000040, dwRecLen = 0x8
<> Record [ 2 ] dwRecAddr = 0x8c000048, dwRecLen = 0x4
<> Record [ 3 ] dwRecAddr = 0x8c001000, dwRecLen = 0x3effc
<> Record [ 4 ] dwRecAddr = 0x8c040000, dwRecLen = 0x1228
<> Record [ 5 ] dwRecAddr = 0x8c043000, dwRecLen = 0xaeac0
<> Record [ 6 ] dwRecAddr = 0x8c0f1ac0, dwRecLen = 0x2753c
<> Record [ 7 ] dwRecAddr = 0x8c119000, dwRecLen = 0x40518
<> Record [ 8 ] dwRecAddr = 0x8c159518, dwRecLen = 0xaae4
<> Record [ 9 ] dwRecAddr = 0x8c164000, dwRecLen = 0x1325d8
<> Record [ 10 ] dwRecAddr = 0x8c2965d8, dwRecLen = 0x5a28
<> Record [ 11 ] dwRecAddr = 0x8c29c000, dwRecLen = 0x12d7b0
<> Record [ 12 ] dwRecAddr = 0x8c3c97b0, dwRecLen = 0x3d848
<> Record [ 13 ] dwRecAddr = 0x8c407000, dwRecLen = 0x3d000
<> Record [ 14 ] dwRecAddr = 0x8c444000, dwRecLen = 0x3dff8
<> Record [ 15 ] dwRecAddr = 0x8c482000, dwRecLen = 0x35ffc
<> Record [ 16 ] dwRecAddr = 0x8c4b8000, dwRecLen = 0x1a000
<> Record [ 17 ] dwRecAddr = 0x8c4d2000, dwRecLen = 0xb2d2c
<> Record [ 18 ] dwRecAddr = 0x8c584d2c, dwRecLen = 0x32d4
<> Record [ 19 ] dwRecAddr = 0x8c588000, dwRecLen = 0x1ca474
<> Record [ 20 ] dwRecAddr = 0x8c752474, dwRecLen = 0x4b8c
<> Record [ 21 ] dwRecAddr = 0x8c757000, dwRecLen = 0x799f4
<> Record [ 22 ] dwRecAddr = 0x8c7d09f4, dwRecLen = 0x216a4
<> Record [ 23 ] dwRecAddr = 0x8c7f3000, dwRecLen = 0x3b0d0
<> Record [ 24 ] dwRecAddr = 0x8c82f000, dwRecLen = 0x37ffc
<> Record [ 25 ] dwRecAddr = 0x8c867000, dwRecLen = 0x1e098
<> Record [ 26 ] dwRecAddr = 0x8c886000, dwRecLen = 0x3bff8
<> Record [ 27 ] dwRecAddr = 0x8c8c2000, dwRecLen = 0x23000
<> Record [ 28 ] dwRecAddr = 0x8c8e5000, dwRecLen = 0x22ae0
<> Record [ 29 ] dwRecAddr = 0x8c908000, dwRecLen = 0x20c0
<> Record [ 30 ] dwRecAddr = 0x8c90b000, dwRecLen = 0x20c0
<> Record [ 31 ] dwRecAddr = 0x8c90e000, dwRecLen = 0x34000
<> Record [ 32 ] dwRecAddr = 0x8c942000, dwRecLen = 0x182b0
<> Record [ 33 ] dwRecAddr = 0x8c95b000, dwRecLen = 0x4ffc
<> Record [ 34 ] dwRecAddr = 0x8c960000, dwRecLen = 0xc6818
<> Record [ 35 ] dwRecAddr = 0x8ca26818, dwRecLen = 0x1da58
<> Record [ 36 ] dwRecAddr = 0x8ca45000, dwRecLen = 0x44
<> Record [ 37 ] dwRecAddr = 0x8ca46000, dwRecLen = 0x1a000
<> Record [ 38 ] dwRecAddr = 0x8ca60000, dwRecLen = 0x405d0
<> Record [ 39 ] dwRecAddr = 0x8caa05d0, dwRecLen = 0x24a30
<> Record [ 40 ] dwRecAddr = 0x8cac5000, dwRecLen = 0x2b000
<> Record [ 41 ] dwRecAddr = 0x8caf0000, dwRecLen = 0x2affc
<> Record [ 42 ] dwRecAddr = 0x8cb1b000, dwRecLen = 0x3fffc
<> Record [ 43 ] dwRecAddr = 0x8cb5b000, dwRecLen = 0x10070
<> Record [ 44 ] dwRecAddr = 0x8cb6c000, dwRecLen = 0x18ffc
<> Record [ 45 ] dwRecAddr = 0x8cb85000, dwRecLen = 0x2c000
<> Record [ 46 ] dwRecAddr = 0x8cbb1000, dwRecLen = 0x3f000
<> Record [ 47 ] dwRecAddr = 0x8cbf0000, dwRecLen = 0x2a000
Hi,
For RNDIS MINI if you have windows ce 6.0 installation you can refer the following path. WINCE600\PUBLIC\COMMON\OAK\DRIVERS\ETHDBG\RNDISMINI\HOST.
Based on your logs I am not understanding whether the BSP you are using is Windows CE 6.0 BSP or CE7.
You have ported a CE 6.0 BSP to OMAP4?
Are you using any reference hardware or customized hardware?
You can change the config.bib but you need to do it carefully. Keeping in mind to change others also.
Regards,
GSR
Hi GSR,
Thanks for your help now I am able to flash the debug build image but the problem now is as debug build is slow so before completing only it is getting rebooted in every 3 minute.
So could you assist that what could be the problem for that. The log I have provided earlier also in this post so after that log only its getting rebooted.
Hi GSR,
Now I am able to build the Debug Build Image and I have a crash in kernel after loading the pm.dll.
Log messages which i am getting are:
PID:00400002 TID:00920006 -OEMIoControl(rc = 1)
PID:00400002 TID:00920006 InitializePMExtension: Can't find 'PmExtPath' key.
PID:00400002 TID:00920006 OSAXST1: >>> Loading Module 'ccfgsvc.dll' (0xC040B1F8) at address 0xEEB10000-0xEEB3D000 in Process 'NK.EXE' (0x90611AD0)
PID:00400002 TID:00920006 DEVICE!RegReadActivationValues RegQueryValueEx(Drivers\BuiltIn\MUsbOtg\DllName) returned 2
PID:00400002 TID:00920006 DEVICE!I_ActivateDeviceEx: can't find all required activation values in 'Drivers\BuiltIn\MUsbOtg'
PID:00400002 TID:00920006 DEVICE!RegReadActivationValues RegQueryValueEx(Drivers\BuiltIn\FlashDisk\DllNamPID:00400002 TID:00920006
PID:00400002 TID:00920006
e) returned 2
PID:00400002 TID:00920006 DEVICE!I_ActivateDeviceEx: can't find all required activation values in 'Drivers\BuiltIn\FlashDisk'
PID:00400002 TID:00500002
After this it is going to IdleState and not launching the shell
Hi William,
Its not available for public. You need to go through TI FAE.
Based on following URL:http://www.windowsfordevices.com/c/a/News/TI-OMAP4430-and-OMAP4460-Windows-Embedded-Compact-7-support/ if you contact Adeneo you may get some hints from them.
Regards,
GSR