Hi.
I have downloaded the ti-sdk-am335x-evm-05.05.01.00-linux-x86. I have flashed the sdk’s u-boot on our AM335x Evaluation Module.
U-Boot works fine with the SYSBOOT configuration SYSBOOT[4:0], 10100b (NAND->NANDI2C->SPI0->EMAC1).
However the U-Boot fails with the SYSBOOT configuration SYSBOOT[4:0], 10101b (NANDI2C->MMC0->EMAC1->UART0). The message “Un-supported Boot Device – 6!!!” is generated (spl.c) and the boot process stops.
Is it correct that there is no support for NANDI2C in the sdk’s u-boot?
Thanks
Peter