This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simulator unique MACID1 and MACID2 is zero

Hi Experts,

after upgrade to CCS 5.3.0 on my Ubuntu 12.04 machine, i try to simulate NETCP with C6670 simulator.

But, the two registers to hold these values, MACID1 (0x02620110) and
MACID2 (0x02620114) are both zero.

Best regards,
Matthias




  • Matthias,

    Yes, this is a simulator, it's not going to have unique MACID.  You'll need to program the MACID that you want to use for the simulation.

    Best Regards,
    Chad

  • Hi Chad,

    i found this website:

    http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#Building_and_running_NDK_client_example_with_simulator

    I alter this file:

    <my ccsv5 install dir>/ccsv5/ccs_base/simulation_keystone1/bin/configurations/tisim_c6670_pv.cfg

    INPUT2    ADAPTOR, ON;

    But MAC is still 00:00:00:00:00:00.

    (Ubuntu 12.04, latest CCSv5 )

    Best Regards,
    Matthias