Other Parts Discussed in Thread: AM3354
In my development board ,i'm using Micron NAND flash ( 2GB ) - 16 Bit.I took a reference design from am335x starter kit but in that doesn't had a NAND flash.So I prefer am335x EVM kit,In that design they were using resistors in the data signals from AD0-AD!5 but denoted as DNI.I get one chinese kit they were using 4.7K resistor in the AD0-AD15 signals.In both the kits they were using the same input power VDDSHV1.
what can i do???if i neglect that resistor what will happens???Current limitation is important there???