Other Parts Discussed in Thread: OMAP-L138
Hi,
In our RRH (Remote radio heads) for 2x2 LTE TDD design , we are using GC5337 & OMAP L138 for DUC,DDC,CFR & DPD functions .
We use an SFP module which interfaces to FPGA , FPGA receives baseband data along with certain other messages(channel activation/deactivation ) after CPRI deframing .
We need to have some interface from FPGA to OMAP to pass on these messages to OMAP ,since OMAP is the master which configures GC5337 & RF .
Can we use GPIO /SPI peripherals of OMAP to interface with FPGA to receive these messages or kindly suggest the alternative
currently on GC5337 eval board ,OMAP interfaces to FPGA and GC via EMIF interface. FPGA receives DPD coefficients from OMAP on this interface.