Reading the TRM descriptions of the SDRAM_TIM_1 and SDRAM_TIM_2 registers, the timings are specified relative to "number of m_clk cycles", where m_clk is the EMIF functional clock running at half the speed of the DDR PLL.
However when I look at the both the StarterWare and u-boot code, as well as the AM335x DDR register spreadsheet, the timings are calculated relative to tCK, which I read to be the full DDR PLL speed.
Is this an error in the TRM, or have I misunderstood something somewhere?
Thanks,
Jonathan