This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDVICP Clock Frequency of DM8165



Hi,

In the datasheet of DM8165 (the datasheet is common for DM816x), it is indicated that the clock frequency depends on the speed range of the chip. The maximum clock frequency of HDVICP is 600MHz for speed range of 2.

Is DM8165 chip available with this speed range? Where can I find the info of what speed ranges are available for each of DM8165, DM8166, DM8167 and DM8168?

 

Thanks in advance!

-Karthik