Hi
I am trying to enable camera in blaze tablet which runs ICS 4A.1.7 release as mentioned in the following link http://www.omappedia.com/wiki/4AI.1.7_OMAP4_Icecream_Sandwich_Release_Notes.
I am using TEVM4XXX-CAM-V1-0 camera kit and connected it to Camera 1 (HDMI style) conector in the tablet.I opened the camera/cameraOMpa4 application in the tablet desktop.It is failing with error saying "Can't connect to the camera" error.
Kindly help me to solve the problem.
Regards
Meenatche