This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fatal error #10296: cannot open output file

Hi all!
I do import the project into CCS3 to CCS5, then I do debug and I go this error fatal error # 10296: cannot open output file what could be the reason that I'm doing wrong?

Import project 
"C:\dvsdk_1_01_00_15\psp_1_00_02_00\pspdrivers\system\dm6437\bios\dm6437_evm\src\video\sample\video_integration\build".

This is repeated with these projects also
video_integrator
raw_capture
loopback
-------------

l"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/lib/DM6437/Debug/rsz_bios_drv.lib" -l"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/lib/DM6437/Debug/vpbe_bios_drv.lib" -l"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/lib/DM6437/Debug/vpfe_bios_drv.lib" -l"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/lib/DM6437/Debug/palos_bios.lib" -l"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/lib/DM6437/Debug/pal_sys_bios.lib" -l"log8.a64P" "../DM6437.cmd" 
<Linking>
fatal error #10296: cannot open output file

>> Compilation failure
"C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/system/dm6437/bios/dm6437_evm
/src/video/sample/video_integration/build/dm6437_evm_bios_vpss_integration_s
ample_out/../../../../../../../../../../system/dm6437/bios/dm6437_evm/src/vi
deo/sample/video_integration/build/Debug/dm6437_evm_bios_vpss_integration_sa
mple_out.out" for writing
gmake: *** [C:/dvsdk_1_01_00_15/psp_1_00_02_00/pspdrivers/system/dm6437/bios/dm6437_evm/src/video/sample/video_integration/build/dm6437_evm_bios_vpss_integration_sample_out/../../../../../../../../../../system/dm6437/bios/dm6437_evm/src/video/sample/video_integration/build/Debug/dm6437_evm_bios_vpss_integration_sample_out.out] Error 1
gmake: Target `all' not remade because of errors.