This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD card probe question ?

[platform] SDK :           dvsdk_2_10_01_18
                  kernel :        Linux IPCAM 2.6.18_pro500-davinci_GV-BX220_1.0
                  Processor: ARM926EJ-S rev 5 (v5l)
                 Hardware  : DM368


1,I have two partitions in SD card.

One of partition is swap and the other used as a storage device. as shown in <1>.

2, I turn on swap partition after, as shown in <2>.

3, I plug out the SD card, then sd card insert.

The partition table has been abnormal. shown as <3>,

Please tell me how to solve this question.

<1>

# cat /proc/partitions

major minor  #blocks  name

 254     0   15558144 mmcblk0

 254     1          1 mmcblk0p1

 254     5   15352848 mmcblk0p5

 254     6     205272 mmcblk0p6

 

# fdisk -l



Disk /dev/mmcblk0: 15.9 GB, 15931539456 bytes

4 heads, 16 sectors/track, 486192 cylinders

Units = cylinders of 64 * 512 = 32768 bytes



        Device Boot      Start         End      Blocks   Id  System

/dev/mmcblk0p1               1      486192    15558136    5  Extended

/dev/mmcblk0p5               1      479777    15352848   83  Linux

/dev/mmcblk0p6          479778      486192      205272   82  Linux swap / Solaris



<2>

# swapon /dev/mmcblk0p6

# cat /proc/swaps

Filename                                Type            Size    Used    Priority

/dev/mmcblk0p6                          partition       205264  0       -1



<3>

# cat /proc/partitions

major minor  #blocks  name

 254     0   15558144 mmcblk0

 

# cat /proc/swaps

Filename                                Type            Size    Used    Priority

/dev/mmcblk0p6\040(deleted)             partition       205264  0       -1

#