Other Parts Discussed in Thread: 66AK2H12
Hi,
Please share application notes/Documents for interfacing Sony ICX274AQ and 66AK2H12 using FPGA or another interface.
Please find attached link of sensor datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: 66AK2H12
Hi,
Please share application notes/Documents for interfacing Sony ICX274AQ and 66AK2H12 using FPGA or another interface.
Please find attached link of sensor datasheet.
Smit,
Any Application Note for interfacing an FPGA to another companies IP (in this case I believe this is a Sony CCD) would need to be from the FPGA vendor. The FPGA would need to be able to support both the CCD and one of our devices IPs for communications.
Best Regards,
Chad
A generic list that we could interface to would be just about all FPGA's available today.
This needs to be narrowed down to which IPs you'd want to interface it to on the DSP side. What kind of data rates are you're going to be needing, etc.
You'd probably be needing FPGA's that would support something like SRIO, PCIe, or SGMII interfaces of the 66AK2H12. So you'd want to look for FPGA's that support your video interfaces and an Interface on the DSP with sufficient bandwidth to support the data. There are only a few FPGA vendors (2 major ones and one or two smaller ones) that are going to be able to support this, and if the FPGA can support the Image Sensor then it most likely will be able to support one of the IP's to interface it to the DSP at the required speeds.
Best Regards,
Chad