Other Parts Discussed in Thread: SYSBIOS
Hi
I conct to dsp on EVM8148 as http://processors.wiki.ti.com/index.php/Connecting_to_DSP_on_C6A8168,_DM8168,_DM8148 said. I create a SYS/BIOS Clock example by CCS4.2.
/*
* ======== clock.c ========
* The clock example shows how to use the ti.sysbios.knl.Clock module to
* create one-shot and periodic Clock Instances. Clock Instances are
* essentially functions that run after a certain number of Clock ticks.
*/
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
Void clk0Fxn(UArg arg0);
Void clk1Fxn(UArg arg0);
/*
* ======== main ========
*/
Void main()
{
Clock_Handle clk2;
Clock_Params clkParams;
/* Create a periodic Clock Instance with period = 5 system time units */
Clock_Params_init(&clkParams);
clkParams.period = 5;
clkParams.startFlag = TRUE;
Clock_create(clk0Fxn, 5, &clkParams, NULL);
/* Create an one-shot Clock Instance with timeout = 11 system time units */
clkParams.period = 0;
clkParams.startFlag = FALSE;
clk2 = Clock_create(clk1Fxn, 11, &clkParams, NULL);
Clock_start(clk2);
BIOS_start();
}
/*
* ======== clk0Fxn =======
*/
Void clk0Fxn(UArg arg0)
{
UInt32 time;
time = Clock_getTicks();
System_printf("System time in clk0Fxn = %lu\n", (ULong)time);
}
/*
* ======== clk1Fxn =======
*/
Void clk1Fxn(UArg arg0)
{
UInt32 time;
time = Clock_getTicks();
System_printf("System time in clk1Fxn = %lu\n", (ULong)time);
System_printf("Calling BIOS_exit() from clk1Fxn\n");
BIOS_exit(0);
}
The program only go into the clk0Fxn but not go into clk1Fxn and clk0Fxn again.Did any more GEL Scripts I should run.
The program works fine on my evm6748.
Thanks for your reply!