This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

profile/level in decoder

Guru 20755 points


Hello,

According to H.264 decoder UG, level API is supported , and profile "always is configured for high profile, independent of value set in this field."
In MPEG-2 and MPEG-4 decoder there is no API for level or profile.
1. Does it mean H.264 decoder will ignore the level in stream and use the level in API ?
2. H.264 decoder support BP,MP,HP, while it said that profile "always is configured for high profile". Isn't there a contradiction here ? Note that BP is not a subset of MP.
3. MPEG-2, MPEG-4 decoders will always use the profile,level from stream ?

Best Regards,

Ran