Other Parts Discussed in Thread: PCF8574
Hi every one.
I boot my dm6446 Evm,this is the output.is it ok???
when I want to run a program,I cant.......what must do??
Loading from NAND 64MiB 1,8V 8-bit, offset 0x2060000
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux.............................................................
.............................................................. done, booting the
kernel.
Linux version 2.6.32-rc2-davinci1 (davinci@localhost.localdomain)
.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Mon Jun 21 16:46:22 IST 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DM644x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm6446a variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 30480
Kernel command line: mem=120M console=ttyS0,115200n8 root=/dev/nfs noinitrd rw n
fsroot=192.168.1.51:/home/mosol2005/targetfs,nolock ip=dhcp davinci_e
_mode=pal davinci_enc_mngr.ch0_output=COMPOSITE video=davincifb:vid0=0,2500K:vid
1=0,2500K:osd0=720x576x16,2025K
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117560KB available (3556K code, 327K data, 124K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 147.86 BogoMIPS (lpj=739328)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 71 gpio irqs
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pcf857x 1-0038: gpios 144..151 on a pcf8574
pcf857x 1-0039: gpios 152..159 on a pcf8574
pcf857x 1-003a: gpios 160..167 on a pcf8574
vpss vpss: dm644x_vpss vpss probed
vpss vpss: dm644x_vpss vpss probe success
ch0 default output "COMPOSITE", mode "PAL"
VPBE Encoder Initialized
LogicPD encoder initialized
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 ch
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport modul
msgmni has been set to 229
io scheduler noop registered
io scheduler anticipatory registered (default)
Console: switching to colour frame buffer device 90x36
davincifb davincifb: dm_osd0_fb: 720x576x16@0,0 with framebuffer size 2025KB
davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 2500KB
davincifb davincifb: dm_osd1_fb: 720x576x4@0,0 with framebuffer size 810KB
davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 2500KB
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownershi
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
console [ttyS0] enabled
serial8250 serial8250.0: unable to register port at index 1 (IO0 MEM1c20400 IRQ4
1): -22
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4
2): -22
brd: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
Read MAC addr from EEPROM: 00:0e:99:02:43:97
Uniform Multi-Platform E-IDE driver
ide-gd driver 1.18
ide0: MMIO-DMA
hda: TOSHIBA MK4032GAX, ATA DISK drive
hda: UDMA/66 mode selected
ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
hda: max request size: 512KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63
hda: cache flushes supported
hda: hda1 hda2
console [netcon0] enabled
netconsole: network logging started
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbtest
i2c /dev entries driver
Linux video capture interface: v2.00
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture: vpss clock vpss_slave enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
tvp514x 1-005d: tvp514x 1-005d decoder driver registered !!
vpfe-capture vpfe-capture: v4l2 sub device tvp514x registered
vpfe_register_ccdc_device: DM6446 CCDC
DM6446 CCDC is registered with vpfe.
Trying to register davinci display video device.
layer=c6672c00,layer->video_dev=c6
Trying to register davinci display video device.
TI UBL Version: 1.50
layer=c6672600,layer->video_dev=c6672770
BootMode = NAND
davinci_init:DaVinci V4L2 Display Driver V1.0 loadedalid magicnum, 0xA1ACED66, found in block 0x00000006
watchdog watchdog: heartbeat 60 sec
DONE
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
U-Boot 2009.03 (Jun
usbcore: registered new interface driver usbhid
I2C: ready
DRAM: 256
usbhid: v2.6:USB HID core driverce: Manufacturer ID: 0xec, Chip
Advanced Linux Sound Architecture Driver Version 1.0.21.
No device for DAI tlv320aic3xIn: serial
Ou
No device for DAI davinci-i2s serial
ARM Clo
asoc: tlv320aic3x <-> davinci-i2s mapping ok
Ethernet PHY: LXT972 @ 0x0
ALSA device list:
Hit an
#0: DaVinci EVM (tlv320aic3
Image Nam
emac-mii: probed+2.6.32-rc1-r37+
eth0: attached PHY driver [LXT971] (mii_bus:phy_addr=1:01, id=1378e2) ARM Linux Kernel Image (uncompressed)
Sending DHCP requests . Data Size: 189388
PHY: 1:01 - Link is Up - 100/Full
Load A
., OK: 800
IP-Config: Got DHCP answer from 192.168.1.1, my address i
Verifying Chec
VFS: Mounted root (nfs filesystem) on device 0:14.1 PREEMPT Mon Jun 21 16:46:22 IST 2010
Freeing init memory: 124K
INIT: version 2.86 bootingJ-S [41069265] revision 5
Please wait: booting...
Starting udev
udev: starting version 141ache, VIVT instruction cac
udevd[966]: inotify_add_watch(3, (null), 10) faichine: DaVinci DM644x E
udevd[966]: inotify_add_watch(3, (null), 10) failed: Bad address
DaVinci dm6446a variant 0x1
udevd[966]: inotify_add_watch(3, (null), 10) failed: Bad address grouping on. Total pages: 30480
udevd[966]: inotify_add_watch(3, (null), 10) failed: Bad addressem=120M console=ttyS0,115200n8 root=/dev/nfs noinitrd rw n
Remounting root file system...
mount: mounting /dev/root on / failed: Invalid arguments,nolock ip=dhcp davinci_enc_mngr.ch0
mount: mounting /dev/root on / failed: Invalid argument
_mode=pal davinci_enc_mngr.ch0_output=COMPOSITE
modprobe: FATAL: Could not open 'kernel/fs/minix/minix.ko': No such file or dire
1=0,2500K:osd0=720x576x16,2025K
ctory
modprobe: FATAL: Could not open 'kernel/fs/minix/minix.ko': No such file or dire
Dentry cache hash table entries: 163
ctory
modprobe: FATAL: Could not open 'kernel/fs/minix/minix.ko': No such file or direodes=1
Hi
ctoryical
EXT2-fs: hda2: couldn't mount because of unsupported optional features (4).nsole: colour dummy device 80x30
Calibrat
kjournald starting. Commit interval 5 seconds
EXT3 FS on hda2, internal journalries: 512
EXT3-fs: recovery complete.te buffer coherency: ok
EXT3-fs: mounted filesystem with writeback data mode.rqs
NET: Registered protocol fam
EXT3 FS on hda1, internal journal
EXT3-fs: recovery complete.s 144..151 on a pcf8574
EXT3-fs: mounted filesystem with writeback data mode.: gpios 152..159 on a pcf8574
ALSA: Restoring mixer settings...: gpios 160..167 on a pcf8574
Setting up IP spoofing protection: rp_filter.pss: dm644x_vpss vpss probed
No state is present for card EVM4x_vpss vpss probe success
Unknown hardware: "tlv320aic3x" "" "" "" ""ult output "COMPOSITE", mode "PAL"
Hardware is initialized using a guess methodr Initialized
LogicP
Configuring network interfaces... /usr/share/alsa/init/default:53: control eer0_1
udhcpc (v1.13.2) startedhdrc musb_hdrc: MUSB HDR
Sending discover...
Sending select for 192.168.1.52...c: new USB bus registered, assigne
Lease of 192.168.1.52 obtained, lease time 259200
usb usb1: configur
adding dns 192.168.1.1choice
done.
INIT: Entering runlevel: 50:1.0: USB hub found
Starting telnet daemon. 1-0:1.0: 1 port detect
modprobe: FATAL: Could not open 'kernel/net/ipv6/ipv6.ko': No such file or direc
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
tory
Starting syslogd/klogd: done
TCP e
Starting thttpd.able entries: 40
_____ _____ _ _
Arago Project http://arago-project.org dm6446-evm ttyS0
Arago 2009.11 dm6446-evm ttyS0