Hi,I have created another thread in ndk helloworld_evm6670l example with an entry function named udp_echo_test which is copied from "ndk_2_21_01_38\packages\ti\ndk\tools\console\conecho.c" . So there are two thread functions now: StackTest() and udp_echo_test(). All I want to do is sending out an udp socket to self and receiving it.
Question 1: I set StackTest() 's priority higher than udp_echo_test()‘s. So the scheduler set up the network stack first and the task hanged when ran to "DaemonNew( SOCK_DGRAM, 0, 7, dtask_udp_hello,...) because no socket is received. Then udp_echo_test() ran and successfully sent out a socket but failed to received the "echo back" socket.The fderror()=61 which means connection refused according to serrno.h. Why is that?
Question 2: I’ve tried to comment the receiving part of udp_echo_test and only sent out the socket . The server function dtask_udp_hello created by DaemonNew successfully received my socket.Can I just receive my udp socket without using daemonNew?
Attach is my helloWorld.c, other files in mcsdk-ndk - helloworld_evm6670l are not modified.
/*
*
* TCP/IP Stack 'Hello World!' Example ported to use BIOS6 OS.
*
* Copyright (C) 2007, 2011 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
//--------------------------------------------------------------------------
// IP Stack 'Hello World!' Example
//
// This is a skeleton application, intended to provide application
// programmers with a basic Stack setup, to which they can start
// adding their code.
//
// To test it as is, use with helloWorld.exe from \winapps directory
//
#include <stdio.h>
#include <ti/ndk/inc/netmain.h>
/* BIOS6 include */
#include <ti/sysbios/BIOS.h>
/* XDC&SYSBIOS includes */
#include <xdc/std.h>
#include <xdc/runtime/IHeap.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Memory.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/heaps/HeapBuf.h>
#include <ti/sysbios/heaps/HeapMem.h>
#include <ti/sysbios/family/c64p/Hwi.h>
#include <ti/sysbios/family/c64p/EventCombiner.h>
#include <xdc/runtime/Log.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Clock.h>
/* Platform utilities include */
#include "ti/platform/platform.h"
#include "ti/platform/resource_mgr.h"
/* Platform Information - we will read it form the Platform Library */
platform_info gPlatformInfo;
#define INVALID_SOCKET (HANDLE)0xFFFFFFFF // Used by socket() and accept()
//---------------------------------------------------------------------------
// Title String
//
char *VerStr = "\nTCP/IP Stack 'Hello World!' Application\n\n";
// Our NETCTRL callback functions
static void NetworkOpen();
static void NetworkClose();
static void NetworkIPAddr( IPN IPAddr, uint IfIdx, uint fAdd );
// Fun reporting function
static void ServiceReport( uint Item, uint Status, uint Report, HANDLE hCfgEntry );
// External references
extern int dtask_udp_hello();
void udp_echo_test();
void StackTest();
//---------------------------------------------------------------------------
// Configuration
//
char *HostName = "tidsp";
char *LocalIPAddr = "192.168.2.100";
char *LocalIPMask = "255.255.255.0"; // Not used when using DHCP
char *GatewayIP = "192.168.2.101"; // Not used when using DHCP
char *DomainName = "demo.net"; // Not used when using DHCP
char *DNSServer = "0.0.0.0"; // Used when set to anything but zero
// Simulator EMAC Switch does not handle ALE_LEARN mode, so please configure the
// MAC address of the PC where you want to launch the webpages and initiate PING to NDK */
Uint8 clientMACAddress [6] = {0x5C, 0x26, 0x0A, 0x69, 0x44, 0x0B}; /* MAC address for my PC */
Task_Params tskParams0;
Task_Params tskParams1;
/*************************************************************************
* @b EVM_init()
*
* @n
*
* Initializes the platform hardware. This routine is configured to start in
* the evm.cfg configuration file. It is the first routine that BIOS
* calls and is executed before Main is called. If you are debugging within
* CCS the default option in your target configuration file may be to execute
* all code up until Main as the image loads. To debug this you should disable
* that option.
*
* @param[in] None
*
* @retval
* None
************************************************************************/
void EVM_init()
{
platform_init_flags sFlags;
platform_init_config sConfig;
/* Status of the call to initialize the platform */
int32_t pform_status;
/*
* You can choose what to initialize on the platform by setting the following
* flags. Things like the DDR, PLL, etc should have been set by the boot loader.
*/
memset( (void *) &sFlags, 0, sizeof(platform_init_flags));
memset( (void *) &sConfig, 0, sizeof(platform_init_config));
sFlags.pll = 0; /* PLLs for clocking */
sFlags.ddr = 0; /* External memory */
sFlags.tcsl = 1; /* Time stamp counter */
#ifdef _SCBP6618X_
sFlags.phy = 0; /* Ethernet */
#else
sFlags.phy = 1; /* Ethernet */
#endif
sFlags.ecc = 0; /* Memory ECC */
sConfig.pllm = 0; /* Use libraries default clock divisor */
pform_status = platform_init(&sFlags, &sConfig);
/* If we initialized the platform okay */
if (pform_status != Platform_EOK) {
/* Initialization of the platform failed... die */
while (1) {
(void) platform_led(1, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
(void) platform_delay(50000);
(void) platform_led(1, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
(void) platform_delay(50000);
}
}
}
//---------------------------------------------------------------------
// Main Entry Point
//---------------------------------------------------------------------
int main()
{
/* create 2 tasks */
Task_Params_init(&tskParams0);
tskParams0.priority = 5;
tskParams0.stackSize = 5120;
Task_create(StackTest, &tskParams0, NULL);
Task_Params_init(&tskParams1);
tskParams1.priority = 4;
tskParams1.stackSize = 5120;
Task_create(udp_echo_test, &tskParams1, NULL);
/* Start the BIOS 6 Scheduler */
BIOS_start ();
}
//
// Main Thread
//
void StackTest()
{
int rc;
int i;
HANDLE hCfg;
QMSS_CFG_T qmss_cfg;
CPPI_CFG_T cppi_cfg;
/* Get information about the platform so we can use it in various places */
memset( (void *) &gPlatformInfo, 0, sizeof(platform_info));
(void) platform_get_info(&gPlatformInfo);
(void) platform_uart_init();
(void) platform_uart_set_baudrate(115200);
(void) platform_write_configure(PLATFORM_WRITE_ALL);
/* Clear the state of the User LEDs to OFF */
for (i=0; i < gPlatformInfo.led[PLATFORM_USER_LED_CLASS].count; i++) {
(void) platform_led(i, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
}
/* Initialize the components required to run this application:
* (1) QMSS
* (2) CPPI
* (3) Packet Accelerator
*/
/* Initialize QMSS */
if (platform_get_coreid() == 0)
{
qmss_cfg.master_core = 1;
}
else
{
qmss_cfg.master_core = 0;
}
qmss_cfg.max_num_desc = MAX_NUM_DESC;
qmss_cfg.desc_size = MAX_DESC_SIZE;
qmss_cfg.mem_region = Qmss_MemRegion_MEMORY_REGION0;
if (res_mgr_init_qmss (&qmss_cfg) != 0)
{
platform_write ("Failed to initialize the QMSS subsystem \n");
goto main_exit;
}
else
{
platform_write ("QMSS successfully initialized \n");
}
/* Initialize CPPI */
if (platform_get_coreid() == 0)
{
cppi_cfg.master_core = 1;
}
else
{
cppi_cfg.master_core = 0;
}
cppi_cfg.dma_num = Cppi_CpDma_PASS_CPDMA;
cppi_cfg.num_tx_queues = NUM_PA_TX_QUEUES;
cppi_cfg.num_rx_channels = NUM_PA_RX_CHANNELS;
if (res_mgr_init_cppi (&cppi_cfg) != 0)
{
platform_write ("Failed to initialize CPPI subsystem \n");
goto main_exit;
}
else
{
platform_write ("CPPI successfully initialized \n");
}
if (res_mgr_init_pass()!= 0) {
platform_write ("Failed to initialize the Packet Accelerator \n");
goto main_exit;
}
else
{
platform_write ("PA successfully initialized \n");
}
// THIS MUST BE THE ABSOLUTE FIRST THING DONE IN AN APPLICATION before
// using the stack!!
//
rc = NC_SystemOpen( NC_PRIORITY_HIGH, NC_OPMODE_INTERRUPT );//NC_PRIORITY_HIGH now is 8
if( rc )
{
platform_write("NC_SystemOpen Failed (%d)\n",rc);
for(;;);
}
// Print out our banner
platform_write(VerStr);
//
// Create and build the system configuration from scratch.
//
// Create a new configuration
hCfg = CfgNew();
if( !hCfg )
{
platform_write("Unable to create configuration\n");
goto main_exit;
}
// We better validate the length of the supplied names
if( strlen( DomainName ) >= CFG_DOMAIN_MAX ||
strlen( HostName ) >= CFG_HOSTNAME_MAX )
{
printf("Names too long\n");
goto main_exit;
}
// Add our global hostname to hCfg (to be claimed in all connected domains)
CfgAddEntry( hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_HOSTNAME, 0,
strlen(HostName), (UINT8 *)HostName, 0 );
// If the IP address is specified, manually configure IP and Gateway
#if defined(_SCBP6618X_) || defined(_EVMTCI6614_) || defined(DEVICE_K2H) || defined(DEVICE_K2K)
/* SCBP6618x, EVMTCI6614, EVMK2H, EVMK2K always uses DHCP */
if (0)
#else
if (!platform_get_switch_state(1))
#endif
{
CI_IPNET NA;
CI_ROUTE RT;
IPN IPTmp;
// Setup manual IP address
bzero( &NA, sizeof(NA) );
NA.IPAddr = inet_addr(LocalIPAddr);
NA.IPMask = inet_addr(LocalIPMask);
strcpy( NA.Domain, DomainName );
NA.NetType = 0;
// Add the address to interface 1
CfgAddEntry( hCfg, CFGTAG_IPNET, 1, 0,
sizeof(CI_IPNET), (UINT8 *)&NA, 0 );
// Add the default gateway. Since it is the default, the
// destination address and mask are both zero (we go ahead
// and show the assignment for clarity).
bzero( &RT, sizeof(RT) );
RT.IPDestAddr = 0;
RT.IPDestMask = 0;
RT.IPGateAddr = inet_addr(GatewayIP);
// Add the route
CfgAddEntry( hCfg, CFGTAG_ROUTE, 0, 0,
sizeof(CI_ROUTE), (UINT8 *)&RT, 0 );
// Manually add the DNS server when specified
IPTmp = inet_addr(DNSServer);
if( IPTmp )
CfgAddEntry( hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_DOMAINNAMESERVER,
0, sizeof(IPTmp), (UINT8 *)&IPTmp, 0 );
}
// Else we specify DHCP
else
{
CI_SERVICE_DHCPC dhcpc;
// Specify DHCP Service on IF-1
bzero( &dhcpc, sizeof(dhcpc) );
dhcpc.cisargs.Mode = CIS_FLG_IFIDXVALID;
dhcpc.cisargs.IfIdx = 1;
dhcpc.cisargs.pCbSrv = &ServiceReport;
CfgAddEntry( hCfg, CFGTAG_SERVICE, CFGITEM_SERVICE_DHCPCLIENT, 0,
sizeof(dhcpc), (UINT8 *)&dhcpc, 0 );
}
//
// Configure IPStack/OS Options
//
// We don't want to see debug messages less than WARNINGS
rc = DBG_WARN;
CfgAddEntry( hCfg, CFGTAG_OS, CFGITEM_OS_DBGPRINTLEVEL,
CFG_ADDMODE_UNIQUE, sizeof(uint), (UINT8 *)&rc, 0 );
//
// This code sets up the TCP and UDP buffer sizes
// (Note 8192 is actually the default. This code is here to
// illustrate how the buffer and limit sizes are configured.)
//
// UDP Receive limit
rc = 8192;
CfgAddEntry( hCfg, CFGTAG_IP, CFGITEM_IP_SOCKUDPRXLIMIT,
CFG_ADDMODE_UNIQUE, sizeof(uint), (UINT8 *)&rc, 0 );
//
// Boot the system using this configuration
//
// We keep booting until the function returns 0. This allows
// us to have a "reboot" command.
//
do
{
rc = NC_NetStart( hCfg, NetworkOpen, NetworkClose, NetworkIPAddr );
} while( rc > 0 );
// Delete Configuration
CfgFree( hCfg );
// Close the OS
main_exit:
NC_SystemClose();
return;
}
void udp_echo_test()
{
SOCKET s;
struct sockaddr_in sin1;
struct sockaddr_in sin2;
int i,tmp,test;
char *pBuf = "Striker!";
UINT32 buffersize = 9;
struct timeval timeout;
/* Allocate the file environment for this task */
fdOpenSession( TaskSelf() );
printf("\n== Start UDP Echo Client Test ==\n");
// Create test socket
s = socket(AF_INET, SOCK_DGRAM, IPPROTO_UDP);
if( s == INVALID_SOCKET )
{
printf("failed socket create (%d)\n",fdError());
goto leave;
}
// We must bind since we won't issue a connect
bzero( &sin1, sizeof(struct sockaddr_in) );
if( bind( s, (PSA) &sin1, sizeof(sin1) ) < 0 )
{
printf("failed bind (%d)\n",fdError());
goto leave;
}
// Prepare address for the SendTo
bzero( &sin1, sizeof(struct sockaddr_in) );
sin1.sin_family = AF_INET;
sin1.sin_len = sizeof( sin1 );
sin1.sin_addr.s_addr = inet_addr(LocalIPAddr);
sin1.sin_port = htons(7);
// Configure our timeout to be 5 seconds
timeout.tv_sec = 5;
timeout.tv_usec = 0;
setsockopt( s, SOL_SOCKET, SO_SNDTIMEO, &timeout, sizeof( timeout ) );
setsockopt( s, SOL_SOCKET, SO_RCVTIMEO, &timeout, sizeof( timeout ) );
// Allocate a working buffer
if( !(pBuf = mmBulkAlloc( 1024 )) )
{
printf("failed temp buffer allocation\n");
goto leave;
}
while(1)
{
if( sendto( s, pBuf, buffersize, 0,(struct sockaddr *)&sin1, sizeof(sin1) ) < 0 )
{
printf("send failed (%d)\n",fdError());
break;
}
else
{
printf("send successful !\n");
}
// Clear the test pattern
mmZeroInit( pBuf, buffersize );
// Try and receive the test pattern back
printf("receiving.... ");
tmp = sizeof(sin2);
if( recvfrom( s, pBuf, buffersize, MSG_WAITALL,(struct sockaddr *)&sin2, &tmp ) < 0 )
{
printf("recv failed (%d)\n",fdError());
break;
}
else
{
printf("recv successful!!!");
}
}
// // Start Test
// for( test=8; test<=1024; test*=2 )
// {
// // Fill buffer with a test pattern
// for(i=0; i<test; i++)
// *(pBuf+i) = (char)i;
//
// // Send the buffer
// printf("Sending %d bytes . ",test);
// if( sendto( s, pBuf, test, 0,(struct sockaddr *)&sin1, sizeof(sin1) ) < 0 )
// {
// printf("send failed (%d)\n",fdError());
// break;
// }
//
// // Clear the test pattern
// mmZeroInit( pBuf, (uint)test );
//
// // Try and receive the test pattern back
// printf("receive . ");
// tmp = sizeof( sin2 );
// if( recvfrom( s, pBuf, test, MSG_WAITALL,(struct sockaddr *)&sin2, &tmp ) < 0 )
// {
// printf("recv failed (%d)\n",fdError());
// break;
// }
//
// // Verify the test pattern
// printf("(");
// ConPrintIPN( sin2.sin_addr.s_addr );
// printf(":%d) verify . ", htons( sin2.sin_port ) );
// for(i=0; i<test; i++)
// if( *(pBuf+i) != (char)i )
// {
// printf("verify failed at byte %d\n",i);
// break;
// }
// if( i==test )
// printf("passed\n");
// }
leave:
if( pBuf )
mmBulkFree( pBuf );
if( s != INVALID_SOCKET )
fdClose( s );
printf("== End UDP Echo Client Test ==\n\n");
}
//
// System Task Code [ Server Daemon Servers ]
//
static HANDLE hHello=0;
//
// NetworkOpen
//
// This function is called after the configuration has booted
//
static void NetworkOpen()
{
// Create our local server
/*
Type Socket type (SOCK_STREAM, SOCK_STREAMNC,orSOCK_DGRAM)
LocalAddress LocalIP address (set to NULL for wild card)
LocalPort LocalPort to serve (can not be NULL)
PCb Pointer to call back to handle server event (connection or activity)
Priority Priority of new task to create for call back function
StackSize Stack size of new task to create for call back function
Argument Argument(besides socket)to pass to call back function
MaxSpawn Maximum number of call back function instances (must be 1 for UDP)
*/
// hHello = DaemonNew( SOCK_DGRAM, 0, 7, dtask_udp_hello,
// OS_TASKPRINORM, OS_TASKSTKNORM, 0, 1 );//its an udp socket
}
//
// NetworkClose
//
// This function is called when the network is shutting down,
// or when it no longer has any IP addresses assigned to it.
//
static void NetworkClose()
{
DaemonFree( hHello );
}
//
// NetworkIPAddr
//
// This function is called whenever an IP address binding is
// added or removed from the system.
//
static void NetworkIPAddr( IPN IPAddr, uint IfIdx, uint fAdd )
{
IPN IPTmp;
if( fAdd )
printf("Network Added: ");
else
printf("Network Removed: ");
// Print a message
IPTmp = ntohl( IPAddr );
printf("If-%d:%d.%d.%d.%d\n", IfIdx,
(UINT8)(IPTmp>>24)&0xFF, (UINT8)(IPTmp>>16)&0xFF,
(UINT8)(IPTmp>>8)&0xFF, (UINT8)IPTmp&0xFF );
}
//
// Service Status Reports
//
// Here's a quick example of using service status updates
//
static char *TaskName[] = { "Telnet","HTTP","NAT","DHCPS","DHCPC","DNS" };
static char *ReportStr[] = { "","Running","Updated","Complete","Fault" };
static char *StatusStr[] = { "Disabled","Waiting","IPTerm","Failed","Enabled" };
static void ServiceReport( uint Item, uint Status, uint Report, HANDLE h )
{
printf( "Service Status: %-9s: %-9s: %-9s: %03d\n",
TaskName[Item-1], StatusStr[Status],
ReportStr[Report/256], Report&0xFF );
//
// Example of adding to the DHCP configuration space
//
// When using the DHCP client, the client has full control over access
// to the first 256 entries in the CFGTAG_SYSINFO space.
//
// Note that the DHCP client will erase all CFGTAG_SYSINFO tags except
// CFGITEM_DHCP_HOSTNAME. If the application needs to keep manual
// entries in the DHCP tag range, then the code to maintain them should
// be placed here.
//
// Here, we want to manually add a DNS server to the configuration, but
// we can only do it once DHCP has finished its programming.
//
if( Item == CFGITEM_SERVICE_DHCPCLIENT &&
Status == CIS_SRV_STATUS_ENABLED &&
(Report == (NETTOOLS_STAT_RUNNING|DHCPCODE_IPADD) ||
Report == (NETTOOLS_STAT_RUNNING|DHCPCODE_IPRENEW)) )
{
IPN IPTmp;
// Manually add the DNS server when specified
IPTmp = inet_addr(DNSServer);
if( IPTmp )
CfgAddEntry( 0, CFGTAG_SYSINFO, CFGITEM_DHCP_DOMAINNAMESERVER,
0, sizeof(IPTmp), (UINT8 *)&IPTmp, 0 );
}
}