Other Parts Discussed in Thread: AM3352
I am using SYS/BIOS version 6.34.2.18 on a AM3352 processor and I'm having an issue of the OS operating very slow. I start my program up which has multiple taska and it will operate correctly. I then pause the execution on the debugger and save some memory to disk and then restart the program. When I restart the program it seems to be spending nearly all of its time in the operating system. I have inserted a dummy idle task and I'm just executing a for loop incrementing a counter. I can start and stop the program and the counter barely moves even though nothing else in the program is running. I have another task which is triggered every 2 ticks (2ms) and it rarely executes.
Does anybody have any ideas about what may be happening?