Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

kworker high cpu load(%80) when playing wav files on ti AM1808, TLV320AIC33, linux board

Other Parts Discussed in Thread: AM1808, TLV320AIC33, OMAP-L138

Hi,

I'm experiencing kworker high CPU usage(%40-80) when playing ."wav" files with aplay command. Using aplay command and executing my own voip application give the same results. CPU load on capture is normal but playback process always consuming high CPU. I changed linux kernel to 2.6.32 from 2.6.36 but similar load appeared on  "/sbin/klogd" and "/sbin/syslogd".

top command output on 2.6.36 kernel :

PID  PPID USER     STAT   VSZ %MEM %CPU COMMAND

1445 2 root RW 0 0% 80% [kworker/0:2]
1444 1442 root R 3036 2% 35% top
1449 1434 root S 3320 3% 0% aplay 8bitpcm.wav

top command output on 2.6.32 kernel:

5 2 root RW 0 0% 33% [events/0]
1371 1 root R 2808 2% 38% /sbin/klogd -n
1369 1 root S 2872 2% 32% /sbin/syslogd -n -C64 -m 20
1388 1386 root R 2984 2% 7% top
1389 1381 root S 3268 3% 1% aplay 8bitpcm.wav

My custom hw is very similar with hawkboard (ti AM1808,TLV320AIC33 audio codec).

Linux version 2.6.36

Advanced Linux Sound Architecture Driver Version 1.0.23.

tlv320aic3x <-> davinci-i2s mapping ok

ALSA device list:
DA850/OMAP-L138 EVM (tlv320aic3x)

An Angstrom distributed file system (UBIFS formated)

root@hawk:~# cat /proc/asound/version
Advanced Linux Sound Architecture Driver Version 1.0.21.

Thanks

Bircan