This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 eZDSP with ADS1298ECG-FE

Hello,

We are trying to implement the MDK using the c5515 ezDSP instead of the C5515 DSP EVM. Is it possible to connect the expansion connector P4 on the ezDSP to J3 on the ADS1298ECG-FE eval to interface the two (via SPI)? Can the software used for the C5515 EVM also be used for the ezDSP and with this setup? 

Sincerely,

Hussam