Hi Folks,
I'm a reletive newbie to the Sitara plaform, i got a a couple of beaglebones and have had a good play with them. Got Debian linux up and running and have them doing some useful stuff. I'm contemplating a couple of product designs now.. Because its christmas i also had enough time to read some stuff and came across the ethercat solution that is on the ICE Development board... I'm really interested in that because it could solve some problems i've had.
Is there a Sitara based Dev system that will allow me to use linux and ether cat? Obvsioulyt he beagleboard won't, it only has one ethernet port! I've ordered the ICE platform, but it seems that running linux on it, is going to be challenging... and i've ordered the TMDSSK3358 - AM335x Starter Kit, which does have two ports, and seems to run linux, but i'm not sure if it supports ethercat..
Does anyone have any wisdom on this they want to share?