This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 is 2GB?

Hi all 

In Mistral 8148 EVM board, have 8pcs DDR3(MT41J128M8JP-125) on two banks(DDR0, DDR1), the total size is 1G bytes.

but when I power on the EVM, the u-boot report DDR3 information is DRAM:  2 GiB, why?

//-----------------------------------------------------------------

U-Boot 2010.06 (Oct 10 2012 - 14:08:25)

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz

DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0

NAND read: device 0 offset 0x20000, size 0x40000
262144 bytes read: OK
## Starting application at 0x81000000 ...