Hi,
I am trying to port android jellybean 4.1.1 (3.0.31 kernel )release on customized board which has more similar hardware architecture as blaze. I am getting an error related to GFX library. I have make sure that, GFX library version for kernel & file system are properly matched.
Error log in logcat:
====================================================================================
V/IMGSRV ( 94): pvrsrvinit complete
D/MDnsDS ( 98): MDnsSdListener::Hander starting up
D/MDnsDS ( 98): MDnsSdListener starting to monitor
D/MDnsDS ( 98): Going to poll with pollCount 1
I/mediaserver( 103): ServiceManager: 0x41a27ce0
I/AudioFlinger( 103): Using default 3000 mSec as standby time.
I/CameraService( 103): CameraService started (pid=103)
D/AndroidRuntime( 101):
D/AndroidRuntime( 101): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 101): CheckJNI is OFF
I/SurfaceFlinger( 100): SurfaceFlinger is starting
I/SurfaceFlinger( 100): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
E/FramebufferNativeWindow( 100): couldn't open framebuffer HAL (Not a typewriter)
E/FramebufferNativeWindow( 100): couldn't open gralloc HAL (Not a typewriter)
E/SurfaceFlinger( 100): Display subsystem failed to initialize. check logs. exiting...
D/AndroidRuntime( 250):
D/AndroidRuntime( 250): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
====================================================================================
Kernel log:
====================================================================================
[ 14.883117] PVR: PVRCore_Init
<6>PVR: PVRSRVDriverProbe(pDevice=c78ac600)
[ 14.892883] PVR: PVRSRVDriverProbe(pDevice=c78ac600)
<6>PVR: SGX register base: 0x56000000
[ 14.901855] PVR: SGX register base: 0x56000000
<6>PVR: SGX register size: 65535
[ 14.912719] PVR: SGX register size: 65535
<6>PVR: SGX IRQ: 53
[ 14.919219] PVR: SGX IRQ: 53
<6>PVR: EnableSystemClocks: Enabling System Clocks
[ 14.928710] PVR: EnableSystemClocks: Enabling System Clocks
<6>PVR: PVRCore_Init: major device 246
[ 14.939056] PVR: PVRCore_Init: major device 246
<6>PVR: Installing MISR with cookie bf040550
[ 15.525848] PVR: Installing MISR with cookie bf040550
<6>cfg80211: Calling CRDA to update world regulatory domain
[ 15.536865] cfg80211: Calling CRDA to update w<6>PrVlR: Insdtal lingr deveigce LISR SuGX aISR ton IRQr 53 ywith c odokie co7a5m8100
ai<6>PVR : OS
UnMapPhysToLin: unmapping 65535 bytes from c8d20000
<6>[PVR: Sys Finalis e: V5e.rsion5 str4ing: SG9X r2ev2i4sion =] 1.2.0P
V R: Installing device LISR SGX ISR on IRQ 53 with cookie c7a58100
[ 15.555206] PVR: OSUnMapPhysToLin: unmapping 65535 bytes from c8d20000
[ 15.561889] PVR: SysFinalise: Version string: SGX revision = 1.2.0
<6>init: command 'insmod' r=0
[ 15.587036] init: command 'insmod' r=0
<6>cfg80211: World regulatory domain updated:
[ 15.633422] cfg80211: World regulatory domain updated:
<6>cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
[ 15.648742] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
<6>cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 15.665252] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 15.682708] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 15.703613] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
<6>cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 15.730529] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 15.761810] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
<6>init: command 'insmod' r=0
[ 17.379394] init: command 'insmod' r=0
<6>init: waitpid returned pid 94, status = 00000000
<5>[init: proce s s 1'pvrsrv7init.', p3id 984 9exit6ed
8] init<:6>in it: awaitipid returned pidt 1p0i0, statusd = r0e000000t0
rned <5>piniti: proce ss '4sur,fac eflsingetr', apid 100 etxitesd
= 0000000<5>init: 0proces s '
surfaceflinger' killing any children in process group
<5>in[it: ser vice 'zy1gote7' i.s being 3k9ille2d
56] init: p<5r>init: starotingc 'zyegote's
s 'pvrsrvini<6>initt:' Crea,ted socpket '/deivd/socket9/z4ygote' withe modxe '660'i, ueser '0d', gro up
'1000'
[ 17.400756] init: waitpid returned pid 100, status = 00000000
[ 17.406616] init: process 'surfaceflinger', pid 100 exited
[ 17.414306] init: process 'surfaceflinger' killing any children in process group
[ 17.419158] init: service 'zygote' is being killed
[ 17.423004] init: starting 'zygote'
====================================================================================