Hi,
I tried to wakeup OMAP4430 ES2.1 Panda from static memory suspend (retention) using serial console uart2 on latest linux-omap master branch, it doesn’t wakeup.
But I could enable wakeup capability bit for GPIO_121 on Panda which wakes up fine from retention.
On the serial uart side I have manually enabled wakeup by echo enabled > /sys/devices/platform/omap_uart.2/tty/ttyO2/power/wakeup
I could verify that before entering static suspend in the idle path the uart irrx pad register is set with wakeup enable bit (1<<14).
Even I posted same mail to linux-omap mailing list but did not get any reply on it. Could someone point me what I could be missing?
Thanks,
Gowda