Kaiqi Yang said:Hi, I am a beginner of AIF on C674, and I download a example project from http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber= sprab58, to meet my requirements, I changed the code a little bit to fulfill an unidirectional transmission from DSP1 to DSP2, and it works. But when I try to trigger another transmission in which DSP2 transfers those data back to DSP1, it never works. Here is my project, anyone knows where is the problem?
Hi Yang,
I am also trying to run the CPRI AIF on the EVMC688. But I see that the Recieve task not getting called. This means that the EDMA transfers not happening. I have use the interdsp example code shared by TI. I have tried both loopback & non loopback. Can you pls tell me if you had done any changes to the example code to make it work ?
Also you have any idea as to why its not working in my case ?
Regards,
Tejas