I am importing a simple project from CCSv3.3 the audioSample from the CSL C6747 to run on OMAP137 using XDS510USB
'Invoking: C6000 Compiler'
1 error
"C:/TI/PSPDrivers_01_20_00/packages/ti/pspiom/examples/evm6747/audio/src/audioSample_io.c", line 52: fatal error #5: could not open source file "ti/sdo/edma3/drv/edma3_drv.h"
2 warnings
Invalid project path: Include path not found (\packages)
Invalid project path: Include path not found (C:\TI\PSPDrivers_01_20_00\include)
I have noticed this line is unresoled
#include "ti/sdo/edma3/drv/edma3_drv.h"
I have CCSv5.3 installed in C:\TI\ with the following
C:\TI\ccsv5
C:\TI\bios_5_42_00_07
C:\TI\bios_6_34_02_18
C:\TI\C674x_dsp_1_00_00_11
C:\TI\grace_2_00_01_65
C:\TI\ipc_1_25_00_04
C:\TI\mcusdk_1_00_01_74
C:\TI\NDK_2_0_0
C:\TI\PSPDrivers_01_20_00
C:\TI\uia_1_01_01_14
C:\TI\xdais_7_21_01_07
C:\TI\xdctools_3_24_05_48
1. Please help to resolve the above include statement
2. please help to eliminate the error + 2 warnings
3. Please advise on else I need to install so that I can run examples from the NDK on CCSv5.3
Thanks for the help