All:
1. I noticed the release notes are titled "C55XCSL - LOWPOWER - 3.00.00.02" - are there specific improvements in the realm of low power? (versus version 2.50?)
2. Also, there is a doc folder with 2 subfolders: csl_api_html and csl_examples_html
However, it is not clear what to "click" inside of the folders to look at the documentation. I clicked on annotated.html and then did "main page" - that was blank. It looks like a starting point may be "files" but there are also "modules" which is pretty confusing at best. Any further help would be appreciated.