We are using a OV5640 sensor in our design and I am unable to run the camera test :
/system/bin/camera_test -f
openCamera(camera_index=0)
Unable to connect to CameraService
Retrying...
Giving up!!
Camera initialization failed
Application closed after: 1014502 ms
I'm guessing this is because of these android logs:
logcat -d |busybox grep -i camera
I/CameraService( 108): CameraService started (pid=108)
E/CameraHal( 108): (40079630) hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXDCC.cpp:99 initDCC - No DCC files found, switching back to default DCC
E/CameraHal( 108): (40079630) hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXDCC.cpp:44 loadDCC - Error in DCC Init
E/CameraHal( 108): (40079630) hardware/ti/omap4xxx/camera/BaseCameraAdapter.cpp:2682 CameraAdapter_Capabilities - supportedCameras= 0
E/CameraHal( 108): (40079630) hardware/ti/omap4xxx/camera/CameraProperties.cpp:108 loadProperties - camera busy. properties not loaded. num_cameras = 0
E/CameraHal( 108): (40079630) hardware/ti/omap4xxx/camera/CameraHal_Module.cpp:750 camera_get_number_of_cameras - Unable to create or initialize CameraProperties
W/PackageManager( 280): Package com.ti.omap4.android.camera desires unavailable shared library com.google.android.media.effects; ignoring!
E/CameraService( 108): CameraService::connect X (pid 805) rejected (invalid cameraId 0).
E/CameraService( 108): CameraService::connect X (pid 805) rejected (invalid cameraId 0).
E/CameraService( 108): CameraService::connect X (pid 818) rejected (invalid cameraId 0).
And the ducati logs indicate that it is looking for a OV5650:
[ 0.884] [ERR=22] src/sensor_detect_MSP.c:[303]:0>>:OV5650 Socket:0
and since we are using a 5640 there is no sensor detected. There is a OV5640 driver in the ducati source so I don't understand why it does not see it. We are using the pre-built ducati firmware that comes with the 4AJ.2.1 release:
[ 0.000] ***DUCATI VERSION INFO***
[ 0.000] Compile DATE Sep 27 2012 TIME 16:29:43
[ 0.000] GIT ducati_mmlegacy
[ 0.000] BRANCH:(no branch) TAG:TI-MM-DUCATI_RLS_2.x.15.2
[ 0.000] COMMIT-ID:36d0068
Is there a version of the ducati firmware with the OV5640 enabled or do I need to build my own?
thank you,
jeff