Other Parts Discussed in Thread: 4460, TWL6030
Hi,
I'm trying to enable the thermal management feature in a board using the 4460 and TWL6030 and am having issues at startup. I get the errors listed below.
In the TWL6030 reference, it mentions the use of an NTC thermistor connected to GPADC_IN1. However, in the Panda Board ES reference, this thermistor is not loaded, yet the thermal management features can still be enabled.
Is this thermistor necessary for the 4460 in order to enable thermal management? If not, can somebody point me to the changes necessary in kernel to get this working?
I am running 4AJ.2.1.
Thanks,
Jason
~~~
[ 6.445983] thermal_sensor_set_temp: no cooling agents for domain cpu
[ 6.453155] omap_report_temp:thermal_sensor_set_temp reports error
[ 6.460418] thermal_sensor_set_temp: no cooling agents for domain cpu
[ 6.460449] omap_temp_sensor omap_temp_sensor.0: omap_ondie_sensor : 'omap_temp_sensor'
[ 6.460723] pcb_temp_sensor pcb_temp_sensor.0: pcb_sensor : 'pcb_temp_sensor'
[ 25.343902] thermal_lookup_temp: getting temp is not supported for domain pcb
[ 25.368011] mvolt_to_temp_conversion:Temp read is invalid 8
[ 25.374328] thermal_lookup_temp: getting temp is not supported for domain pcb
[ 25.399353] mvolt_to_temp_conversion:Temp read is invalid 0
[ 25.405670] thermal_lookup_temp: getting temp is not supported for domain pcb
[ 26.422912] mvolt_to_temp_conversion:Temp read is invalid 0