Hi ,guys! Recently I am using NDK to fulfill the communication between C6474 with Linux system. C6474 is used as the Server and Linux system is used as the Client .When the amount of transfered data is small, the communication is success. But if the amount of transfered data grows bigger, which means the receiver should receive the data serveral times with recv() function, part of the received data is incorrect. What is the possible problem?