Hi,we buy a Spectrum Digital DM816x/AM389x EVM (with daughter card)。That is OK, but one day I typed “ nand scrub ” in uboot,then uboot has a bug. I think that is because nand flash has been cleared all ,so I reload uboot file again in CCS5 following the guide in DVRRDK,as follows:
turn SW3 to all“0”,SW4[10],open CCS5.2 ,reload the project in host-tools/src/ nand-flash-writer. After rebuild,I reload the nand-flash-writer.out into the board,and start。Then we can see taht:
[CortexA8] Welcome to CCS Nand Flash Utility
[CortexA8]
[CortexA8] Choose your operation
[CortexA8] Enter 1 ---> To Flash an Image
[CortexA8] Enter 2 ---> To ERASE the whole NAND
[CortexA8] Enter 3 ---> To EXIT
2
[CortexA8] Starting NETRA NAND writer
[CortexA8]
[CortexA8] ----------------------
[CortexA8] NAND FLASH DETAILS
[CortexA8] ----------------------
[CortexA8] Device ID : 0xca
[CortexA8] Manufacture ID : 0x2c
[CortexA8] Page Size : 2048 Bytes
[CortexA8] Spare Size : 64 Bytes
[CortexA8] Pages_Per_Block : 64
[CortexA8] Number_of_Blocks : 2048
[CortexA8] Device_width : 2 Byte
[CortexA8] DeviceSize : 256 MB
[CortexA8]
[CortexA8] Performing Global Nand Erase
[CortexA8] ... done
[CortexA8]
[CortexA8] NAND flashing successful!
[CortexA8] Welcome to CCS Nand Flash Utility
[CortexA8]
[CortexA8]
[CortexA8] Choose your operation
[CortexA8] Enter 1 ---> To Flash an Image
[CortexA8] Enter 2 ---> To ERASE the whole NAND
[CortexA8] Enter 3 ---> To EXIT
1
[CortexA8] Enter image file path
E:\my\sharedfiles\DVRRDK_03.00.00.00\pre_built_binary\ti816x_dvr\uboot_NAND_DM816X_DVR
[CortexA8] Enter offset (in hex):
0
[CortexA8] Choose the ECC scheme from given options :
[CortexA8] Enter 1 ---> BCH 8-bit
[CortexA8] Enter 2 ---> HAM
[CortexA8] Enter 3 ---> T0 EXIT
[CortexA8] Please enter ECC scheme type :
1
[CortexA8] Starting NETRA NAND writer
[CortexA8]
[CortexA8] ----------------------
[CortexA8] NAND FLASH DETAILS
[CortexA8] ----------------------
[CortexA8] Device ID : 0xca
[CortexA8] Manufacture ID : 0x2c
[CortexA8] Page Size : 2048 Bytes
[CortexA8] Spare Size : 64 Bytes
[CortexA8] Pages_Per_Block : 64
[CortexA8] Number_of_Blocks : 2048
[CortexA8] Device_width : 2 Byte
[CortexA8] DeviceSize : 256 MB
。。。。。。。。。
[CortexA8] Writing image data to Block 1 Page0x1f
[CortexA8] Writing image data to Block 1 Page0x20
[CortexA8] Writing image data to Block 1 Page0x21
[CortexA8] Image successfully flashed
[CortexA8]
[CortexA8]
[CortexA8] NAND flashing successful!
So Uboot reloads successfully ,then we turn SW3 to [0000010010],and start the board, it goes into uboot. But when we type “nand erase”in uboot ,we get the bug information that :
Also ,I try to save the uboot enviroment,and the bug information goes that :

Then ,it comes a waiting without stop,so I can do nothing。
I also think that I do not have reloaded the right uboot bin ,so I erase all, and reload bellow
E:\my\sharedfiles\DVRRDK_03.00.00.00\pre_built_binary\ti816x_dvr\uboot_NAND_DM816X_EVM
But , the bug information is also here ,this is no chang.
What is the matter ?/ what can I do ? please help me
Thank you !!
Best wishes !