This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4430 Debug Build not Booting up.



Hi All ,

I am performing the Debug and Release build for OMAP4430 BSP for Panda Board.

So in that case release build is working fine but in debug build I am getting log as mentioned below and then its not booting up completely.

Windows CE SD X-Loader for OMAP4430
Built Jan  4 2013 at 10:36:22
Version 6.13.00
open ebootsd.nb0 file

jumping to ebootsd image

Microsoft Windows CE Bootloader Common Library Version 1.4 Built Jan  4 2013 11:31:49

Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Jan  4 2013 at 11:36:56
EBOOT Version 1.5, BSP 6.13.00
BEFORE RETURN System ready!
Preparing for download...
INFO: Predownload....
WARN: Boot config wasn't found, using defaults
INFO: SW4 boot setting: 0x05

 After default boot configuration
>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...

--------------------------------------------------------------------------------
 Main Menu
--------------------------------------------------------------------------------
 [1] Show Current Settings
 [2] Select Boot Device
 [3] Select KITL (Debug) Device
 [4] Network Settings
 [5] SDCard Settings
 [6] Set Device ID
 [7] Save Settings
 [8] Flash Management
 [0] Exit and Continue

 Selection: 2

--------------------------------------------------------------------------------
 Select Boot Device
--------------------------------------------------------------------------------
 [1] LAN9115 MAC
 [2] USBFn RNDIS
 [3] NK from SDCard FILE
 [0] Exit and Continue

 Selection (actual LAN9115 MAC): 3
 Boot device set to NK from SDCard FILE

--------------------------------------------------------------------------------
 Main Menu
--------------------------------------------------------------------------------
 [1] Show Current Settings
 [2] Select Boot Device
 [3] Select KITL (Debug) Device
 [4] Network Settings
 [5] SDCard Settings
 [6] Set Device ID
 [7] Save Settings
 [8] Flash Management
 [0] Exit and Continue

 Selection: 0

BL_IMAGE_TYPE_BIN

Download file information:
-----------------------------------------------------------
[0]: Address=0x8c000000  Length=0x03462a18  Save=0x80000000
-----------------------------------------------------------
Download file type: 1
 <> Record [ 0 ] dwRecAddr = 0x8c000000, dwRecLen = 0x4
 <> Record [ 1 ] dwRecAddr = 0x8c000040, dwRecLen = 0x8
 <> Record [ 2 ] dwRecAddr = 0x8c000048, dwRecLen = 0x4
 <> Record [ 3 ] dwRecAddr = 0x8c001000, dwRecLen = 0x3effc
 <> Record [ 4 ] dwRecAddr = 0x8c040000, dwRecLen = 0x1228
 <> Record [ 5 ] dwRecAddr = 0x8c043000, dwRecLen = 0xaeac0
 <> Record [ 6 ] dwRecAddr = 0x8c0f1ac0, dwRecLen = 0x2753c
 <> Record [ 7 ] dwRecAddr = 0x8c119000, dwRecLen = 0x40518
 <> Record [ 8 ] dwRecAddr = 0x8c159518, dwRecLen = 0xaae4
 <> Record [ 9 ] dwRecAddr = 0x8c164000, dwRecLen = 0x1325d8
 <> Record [ 10 ] dwRecAddr = 0x8c2965d8, dwRecLen = 0x5a28
 <> Record [ 11 ] dwRecAddr = 0x8c29c000, dwRecLen = 0x12d7b0
 <> Record [ 12 ] dwRecAddr = 0x8c3c97b0, dwRecLen = 0x3d848
 <> Record [ 13 ] dwRecAddr = 0x8c407000, dwRecLen = 0x3d000
 <> Record [ 14 ] dwRecAddr = 0x8c444000, dwRecLen = 0x3dff8
 <> Record [ 15 ] dwRecAddr = 0x8c482000, dwRecLen = 0x35ffc
 <> Record [ 16 ] dwRecAddr = 0x8c4b8000, dwRecLen = 0x1a000
 <> Record [ 17 ] dwRecAddr = 0x8c4d2000, dwRecLen = 0xb2d2c
 <> Record [ 18 ] dwRecAddr = 0x8c584d2c, dwRecLen = 0x32d4
 <> Record [ 19 ] dwRecAddr = 0x8c588000, dwRecLen = 0x1ca474
 <> Record [ 20 ] dwRecAddr = 0x8c752474, dwRecLen = 0x4b8c
 <> Record [ 21 ] dwRecAddr = 0x8c757000, dwRecLen = 0x799f4
 <> Record [ 22 ] dwRecAddr = 0x8c7d09f4, dwRecLen = 0x216a4
 <> Record [ 23 ] dwRecAddr = 0x8c7f3000, dwRecLen = 0x3b0d0
 <> Record [ 24 ] dwRecAddr = 0x8c82f000, dwRecLen = 0x37ffc
 <> Record [ 25 ] dwRecAddr = 0x8c867000, dwRecLen = 0x1e098
 <> Record [ 26 ] dwRecAddr = 0x8c886000, dwRecLen = 0x3bff8
 <> Record [ 27 ] dwRecAddr = 0x8c8c2000, dwRecLen = 0x23000
 <> Record [ 28 ] dwRecAddr = 0x8c8e5000, dwRecLen = 0x22ae0
 <> Record [ 29 ] dwRecAddr = 0x8c908000, dwRecLen = 0x20c0
 <> Record [ 30 ] dwRecAddr = 0x8c90b000, dwRecLen = 0x20c0
 <> Record [ 31 ] dwRecAddr = 0x8c90e000, dwRecLen = 0x34000
 <> Record [ 32 ] dwRecAddr = 0x8c942000, dwRecLen = 0x182b0
 <> Record [ 33 ] dwRecAddr = 0x8c95b000, dwRecLen = 0x4ffc
 <> Record [ 34 ] dwRecAddr = 0x8c960000, dwRecLen = 0xc6818
 <> Record [ 35 ] dwRecAddr = 0x8ca26818, dwRecLen = 0x1da58
 <> Record [ 36 ] dwRecAddr = 0x8ca45000, dwRecLen = 0x44
 <> Record [ 37 ] dwRecAddr = 0x8ca46000, dwRecLen = 0x1a000
 <> Record [ 38 ] dwRecAddr = 0x8ca60000, dwRecLen = 0x405d0
 <> Record [ 39 ] dwRecAddr = 0x8caa05d0, dwRecLen = 0x24a30
 <> Record [ 40 ] dwRecAddr = 0x8cac5000, dwRecLen = 0x2b000
 <> Record [ 41 ] dwRecAddr = 0x8caf0000, dwRecLen = 0x2affc
 <> Record [ 42 ] dwRecAddr = 0x8cb1b000, dwRecLen = 0x3fffc
 <> Record [ 43 ] dwRecAddr = 0x8cb5b000, dwRecLen = 0x10070
 <> Record [ 44 ] dwRecAddr = 0x8cb6c000, dwRecLen = 0x18ffc
 <> Record [ 45 ] dwRecAddr = 0x8cb85000, dwRecLen = 0x2c000
 <> Record [ 46 ] dwRecAddr = 0x8cbb1000, dwRecLen = 0x3f000
 <> Record [ 47 ] dwRecAddr = 0x8cbf0000, dwRecLen = 0x2a000