This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HexAIS_OMAP-L138 vs AISgen

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

I am using c6748.

I generate my AIS binary file with AISGEN and can boot it from SPI flash.

In the AISgen, I only specify the boot mode, device type, clock course(24MHz). I do not specify anything else.

it still works, I mean the code still boots.

 

I try to do the same with HexAIS_OMAP-L138.

But booting does not occur. My .ini file is below.

 

COuld you suggest possible causes for this?

Best regards

 

 

 

 

[General]

; SPIMASTER,I2CMASTER,EMIFA,NAND,EMAC,UART,PCI,HPI,USB,MMC_SD,VLYNQ,RAW

BootMode=SPIMASTER seqReadEn=TRUE

; 8,16,24 - used for SPI,I2C

AddrWidth=24   

[INPUTFILE]

FILENAME=MXLf.out

; NO_CRC,SECTION_CRC,SINGLE_CRC

crcCheckType=NO_CRC

 

 

 

 

; This section should be used in place of PLL0CONFIG when ; the I2C, SPI, or UART modes are being used.  This ensures that ; the system PLL and the peripheral's clocks are changed together. ; See PLL0CONFIG section for the format of the PLL0CFG fields. ; See PERIPHCLKCFG section for the format of the CLKCFG field. [PLLANDCLOCKCONFIG]

PLL0CFG0 = 0x010E0001

PLL0CFG1 = 0x00000206

PERIPHCLKCFG = 0x00000005