Other Parts Discussed in Thread: TMS320C6474
Hi all,
i want to port my code from the dsp 6474 to the new dsp 6678 ,i am using the Mcbsp port in the old dsp and it not found in the new one any more .
the Mcbsp generate the frame for the HW side from clk of 62.5 Mhz and i am using the both ports with total data transfer of 125Mbps , the frame generated from the McBsp is used in the HW side .
after reading about the 6678 i found that there is TSIP port but because the clk used in this protocol is const(8.163/16.326/32.768 Mhz) i can't use it .
more info :my old dsp 6474 is in the TMS320C6474 Evaluation Module and the new dsp is in the TMDXEVM6678 Evaluation Module .
Is it true that the TSIP port work only with 8.163/16.326/32.768 Mhz clks?
what can replace the McBsp in the new evm board?
Thanks