Hi,
I am running the EDMA3 example with C6678LE EVM which has XDS 560v2 emulation interface. I have checked the target and gel file without solution to the error, see below please. Due to limited C drive space, the projects are in drive E. This could be a problem?
The projects are uploaded in this post.
Could you help me to find out the problem?
Thanks,
.............
C66xx_0: GEL Output: Setup_Memory_Map...
C66xx_0: GEL Output: Setup_Memory_Map... Done.
C66xx_1: GEL Output: Setup_Memory_Map...
C66xx_1: GEL Output: Setup_Memory_Map... Done.
C66xx_2: GEL Output: Setup_Memory_Map...
C66xx_2: GEL Output: Setup_Memory_Map... Done.
C66xx_3: GEL Output: Setup_Memory_Map...
C66xx_3: GEL Output: Setup_Memory_Map... Done.
C66xx_4: GEL Output: Setup_Memory_Map...
C66xx_4: GEL Output: Setup_Memory_Map... Done.
C66xx_5: GEL Output: Setup_Memory_Map...
C66xx_5: GEL Output: Setup_Memory_Map... Done.
C66xx_6: GEL Output: Setup_Memory_Map...
C66xx_6: GEL Output: Setup_Memory_Map... Done.
C66xx_7: GEL Output: Setup_Memory_Map...
C66xx_7: GEL Output: Setup_Memory_Map... Done.
IcePick_D: GEL: File: E:\ti\workspace_v5_1_C6678\edma3_drv_bios6_c6678_st_sample\Debug\edma3_drv_bios6_c6678_st_sample.out Does not match the target type, not loaded.