Hi,
I saw in the AM335X Technical Reference Manual, Table 13-2. LCD Controller Clock Signals, the maximum LCD_CLK is 200MHz, but in the AM335X EVM code, the LCD_CLK is set to 300MHz
/* DISP Freq is 300 MHZ */
/* Set Fdll = 600 MHZ , Fdll = M * 2 * CLKINP/ N + 1; clkout = Fdll /(2 * M2) */
#define DISPPLL_M 25
#define DISPPLL_N 1
#define DISPPLL_M2 1
I just wonder if the LCD_CLK can work reliably at 300MHz?
Thanks,