This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5504 Asynchronous SRAM interface

Guru 10750 points

Hi,

- I assume that in the C5504 User Guide Table 6-20 "EMIF Asynchronous Memory" in the case of SYSCLK = 150MHz E is equal to 6.66nS is that correct?

- Does the Asynchronous SRAM have the SDRAM 100MHz limitation?

- Can I change the Asynchronous SRAM parameters during system operation?

Thanks,

HR