i am using omap l138 and using uart with EDMA.
But the problem is that when i write 1 in FCR register of uart 2 for DMAMODE1 enable bit it will not 1 how to set this bit and why this bit is not set.
using c6748 starter ware drivers.
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i am using omap l138 and using uart with EDMA.
But the problem is that when i write 1 in FCR register of uart 2 for DMAMODE1 enable bit it will not 1 how to set this bit and why this bit is not set.
using c6748 starter ware drivers.
thanks
Rana,
Have you figured out a solution for this? We did not do a good job getting a response to you. Sorry.
Did you find in the UART documentation where it says that the FCR register is write-only, so you cannot read it to see whether DMAMODE1 has been set or not.
Do you have the operations working that you were trying to implement?
Regards,
RandyP