This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c5535 ezdsp : C5535 running at 12.288 MHz as well as FTDI



Hello,

I need to run the C5535 on the C5535 ezDSP board at 12.288 MHz using the CLKIn input. So I have 2 options :

1) replace the original 12 MHz oscillator with my 12.288 MHz source : the FT2232HL (XDS100-V2 INTERFACE) will run at 12.288 MHz rather than 12.000 MHz => is it a problem ?

2) keep the origianl 12 MHz oscillator for the FT2232HL (XDS100-V2 INTERFACE), and tie my external 12.288 MHz oscillator to C5535 CLKIN. In that case, both IC won't run at the same speed => is it a problem ?

Thanks for your comments

Nicolas