This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two cameras share a CSI bus.

We have an Omap4460 based platform that has 3 cameras. We have the camera on Socket 0 and Socket 1, both share the CSI2A. Camera on Socket 0 uses CSI2A pin 1, 2 and 3. Camera on Socket 1 uses CSI2A pin 4 and 5. The CSI2A pin 1 and pin 4 are configured as clock pin, the rest pins are data pins. The camera on Socket 0 works fine. I am having problem with the second camera. It can't be initialized correctly.

Does the current Ducati frame work support the configuration described above? If not, any alternative approaches.

Thanks.

Chao