Hello,
I'd like to boot BeagleBoard with kernel downloaded via Ethernet. I tried use my USB ETH adapter in U-Boot. Following U-Boot README files I added into beagle.h file this:
#define CONFIG_USB_HOST_ETHER /* Enable USB Ethernet adapters */
#define CONFIG_USB_ETHER_ASIX /* Asix, or whatever driver(s) you want */
#define CONFIG_CMD_NET
#define CONFIG_CMD_PING
#define CONFIG_CMD_DHCP
#define CONFIG_BOOTP_SUBNETMASK
#define CONFIG_BOOTP_GATEWAY
#define CONFIG_BOOTP_HOSTNAME
#define CONFIG_BOOTP_BOOTPATH
and into asix.c file this:
{ 0x9710, 0x7830, FLAG_TYPE_AX88172}
, I based on what my host Linux showed to me:
Vendor specific, USB Revision 2.0- Moschip Semiconductor UA0025C 6e003e8f - Class: Vendor specific - PacketSize: 64 Configurations: 1 - Vendor: 0x9710 Product 0x7830 Version 1.0 Configuration: 1 - Interfaces: 1 Bus Powered Remote Wakeup 500mA Interface: 0 - Alternate Setting 0, Endpoints: 3 - Class Vendor specific - Endpoint 1 In Bulk MaxPacket 512 - Endpoint 2 Out Bulk MaxPacket 512 - Endpoint 3 In Interrupt MaxPacket 16 Interval 1ms
But U-Boot don't see it as Ethernet Device, it only recognize it in tree:
(Re)start USB...
USB0: USB EHCI 1.00
scanning bus 0 for devices... 2 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
scanning usb for ethernet devices... 0 Ethernet Device(s) found
OMAP3 beagleboard.org # usb tree USB device tree: 1 Hub (480 Mb/s, 0mA) | u-boot EHCI Host Controller | +-2 Vendor specific (480 Mb/s, 500mA) Moschip Semiconductor UA0025C 6e003e8f
Could you help me with this, please?