Other Parts Discussed in Thread: OMAPL138
When I using JFFS2 on NAND Flash,my program using dsplink can't work,and comes with some error like "Alignment trap: thttpd (844) PC=0x00014bf8 Instr=0xe5950010 Address=0xac457356 FSR 0x001".If I run any other program without using dsplink ,the system can works properly.
But when I using NFS,everything can works properly.
Please help me to solve this problem.Thanks!
PS:
My linux kernel is 2.6.33.
Dsplink version is 1.65.00.02.
I'm using OMAPL138 .
Both mounting way use the same root file system.