This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If the AM3359 get a signal can from active change to standby or deepsleep,I want to design a schematic ,whe the AM3359 is run active I press a button trigger the AM3359

Other Parts Discussed in Thread: AM3359

If the AM3359 get a signal  can  from active  change to standby or deepsleep,I want to design a schematic ,whe the AM3359 is run active  I press a button trigger the AM3359 change to standby or deepsleep .If I only can connect the switch button to the AM3359's GPIO0 ,then when I press the button one time the AM3359 run to standby .

And while the AM3359  is in standby or deepsleep status ,I press the same button that connect to GPIO0 ,I can wakeup the AM3359?