This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DEI OMX Component issue



Hi,

I am trying to Encode two h264 streams, with the single capture.

for this i have created and connected the Omx componet in the following manner

              YUV 420                             YUV 422                                    YUV422

Capture------> DEI (Primary)-----------------> DEI (Secondary) ------------> (Display)

                                  |  Yuv 420                                   | YUV 420

                                  \|/                                                 \|/

                         Encoder (1)                               Encoder (2)

while trying to set the I/P Port parameter of the DEI (secondary)

I am getting this error ( unrecoverable error: OMX_ErrorInsufficientResources (0x80001000) )

any Idea ?

Log file attached "This Log file is created using the command "../ti-uia/loggerSMDump.out 0x9E400000 0x100000 all"

5722.test_deiH.txt

Thanks in advance.